Outputs Blocks
Overview
The FBD editor uses various outputs blocks accessible through the bar in the Toolbox:
|
Block |
Description |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Register Bit Out Block
The
block is used to set an LTMT
main unit register bit value to 0 or 1 from the LTMT
main unit registers.
Register Word Out Block
The
block is used to set an LTMT
main unit register value from the LTMT
main unit registers.
Register NV Bit Out Block
The
block is used to set a non-volatile
register bit value to 0 or 1.
Register NV Word Out Block
Register Temp Bit Out Block
The
block is used to set a temporary
register bit value to 0 or 1.