Start Curve
Overview
The Start Curve tab displays the graph of the motor current (I) during the motor starting time and at sample time intervals. The Start Curve tab is used to analyze the motor starting characteristics from the curve.
The start curve data will be erased from the device after performing a factory reset.
Reference Curve
The plotted curve can be set as the reference curve by clicking Set as Ref.. The reference curve will remain the same until a new curve is set as reference. The blue graph line represents the reference curve.
Zoom Display Options
The following options are available:
-
Zoom Out: To see more program at once.
-
Zoom In: To focus on the specific program in detail.
-
Zoom Area: To have a customized view of the program.
Key Buttons
-
Full Load Current: Displays the full load current value in Amperes.
-
Timestamp: Displays the motor start time.
-
Plot: Reads the latest values and refreshes the motor start characteristics curve.
-
Save: Captures the screen shot of the motor start characteristics curve and allows you to save it to the PC.
-
Set As Ref.: Sets actual curve as reference curve.