Initialization and Connection
Initialization
When you connect the LTMT main unit to the PC, the controller automatically initializes. This initialization process enables the controller and the PC to exchange identification information.
During this process, the custom logic editor indicates wait until initialization is complete.
Connection
After initialization, the LTMT main unit should automatically connect to the PC.
To verify that the controller is connected, check the status bar in the custom logic editor.
If the status bar reads , then select or select icon.
A progress bar briefly appears as your PC connects to the controller, and the word Connected appears in the status bar when the connection process successfully completes.
When the LTMT main unit is connected, you can:
-
Upload customized program files from the controller to SoMove software with the TeSys Tera DTM Library for editing.
-
Download edited customized program files from SoMove software with the TeSys Tera DTM Library to the controller.