DOCA0275EN-01

Tool Bar

Description

The tool bar, at the top of the working space directly below the menu bar, is specific to the TeSys Tera DTM Library:

A Control panel
B Refresh
C Synchronization data area
D Trip and Alarm count display area

Control Panel

To access the Control Panel, select on the tool bar.

The Control Panel appears at the bottom of the window.

The Control Panel displays the following parameters:

  • Device status

  • Motor status

  • Mode status

  • Motor stop cause

  • Trip status

  • Time to cool when motor is stopped or tripped

The Control Panel allows you to perform the following actions:

  • Provide motor commands (Start/Stop)

  • Trip reset

  • Clear command

  • Reset command

Refresh

The option on the tool bar refreshes all the parameters under the Parameter List tab.

Synchronization Data Area

The synchronization data area displays the synchronization status of the data between the LTMT main unit and the PC.

When the LTMT main unit is in the connected mode, displayed data is automatically synchronized.

Mode

Icon

Description

Disconnected

The LTMT main unit is not synchronized with the PC:

  • Parameters list headers and synchronization data area are blue.

  • Parameters are not read in real time from the LTMT main unit

    .
  • All settings can be modified as in configuration mode.

  • You should perform Store to Device operation to write the settings to the device. To save this setting, you have to save the project.

Connected

The LTMT main unit is synchronized with the PC:

  • Parameters list headers and synchronization data area are orange.

  • Parameters displayed are read in real time from the LTMT main unit

  • Modified parameters are written to device on confirmation.

Trip and Alarm Count Display

This area displays the total number of Trip and Alarm in the project.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?