Introducing Custom Logic Editor
Overview
The custom logic editor is a feature of SoMove software with the TeSys Tera DTM Library. Use the custom logic editor to view an existing program file or to create a program file using an instruction based text language, rather than a graphics based programming language.
Editing Custom Logic Program
The easiest way to create a customized program is to begin with the pre-defined program of one of the operating modes (or motor starter type). The installation of the custom logic editor comes with 11 pre-defined program files, one for each motor starter type.
Each program file bears a descriptive name (e.g. DIRECT_ONLINE) and a file extension of *.rtf.
Custom Logic Editor User Interface
To open the custom logic editor, select .
The custom logic editor is available regardless of whether the TeSys Tera DTM Library is in connected mode. However, the transfer of programs between the TeSys Tera DTM Library and the device works only in connected mode.