DOCA0275EN-01

Status Bar

Objective

The status bar, at the bottom of the working space, displays the current status of the LTMT main unit and information related to SoMove software. For more information on the status bar, refer to SoMove Online Help.

Description

A

Connection status

B

Data source

C

Specific message zone

D

Project status

Connection Status

The Connection Status indicates the connection mode between the LTMT main unit and the PC:

Mode

Icon

Description

Disconnected

The LTMT main unit is not connected to the PC.

Disturbed

The connection between the LTMT main unit and the PC is lost.

Connected

The LTMT main unit is connected to the PC.

Data Source

The Data Source indicates the current mode of data. The following tables describes the data source modes:

Mode

Icon

Description

Data set

The parameter values in the data set can be modified in connected mode.

Data set or device locked

The device is protected in connected mode.

Device

The device data set contains information.

Device/Data set

All parameter values are stored to both data sources.

Specific Message Zone

Depending on the fieldbus used for communicating with the device, the specific message zone displays the IP or device address, COM port details and so on.

Project Status

The status of the SoMove software project can be:

  • Project Loaded: Project is displayed in the working space.

  • No Project Open: Project working space is empty.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?