Diagnostics
Overview
The Diagnostics tab displays the motor status, alarm or trip status, logs, device internal status, communication status, and trip counters information of the TeSys Tera system.
The data in this tab is only significant in the connected mode.
The data in the Diagnostics tab is dynamic and refreshes every 1 second except for Logs node.
Description
The following parameters are displayed in the Diagnostics tab:
-
Motor or Load Status
-
Alarm or Trip Status
-
Logs of the TeSys Tera system which includes:
-
Events
-
Device Internal
-
Trips
-
-
Device Internal Status
-
Communication Status
-
Trip Counters
Motor or Load Status
The Motor Status or Load Status window displays the parameters of the configured motor or heater respectively.
The following motor parameters are displayed under the Motor Status or Load Status window:
-
Motor Stop Cause: Reason for stopping the motor operation.
-
Total Active Power: Total power consumed during the motor or heater operation.
-
Motor Status or Load Status:
Current status of the motor or heater. -
Total Run Hour: Total operational time of the motor or heater.
-
Number of Starts: Total number of starts of the motor or heater.
Alarm or Trip Status
The Alarm or Trip Status window displays the status of motor parameters with respect to alarm or trip.
The required parameter can be searched by adding keywords in the search box, selecting the required option under the In drop-down list and by selecting Search.
Logs
The Logs window displays the logs for the following categories:
-
Events
-
Device Internal
-
Trips
Events
The Events window displays the list of event records for the TeSys Tera system.
Up to 100 event logs with record ID, timestamp, event description, and event code will be displayed on the window. Record ID 1 is the latest event recorded and Record ID 100 is oldest event recorded. If there are 100 event logs on the window and if a new event occurred, then the oldest event will be removed from the list and the new event will be added at the top of the list.
Device Internal
The Device Internal window provides the list of internal relay events of the TeSys Tera system.
Up to 20 internal relay logs with record ID, timestamp, event description, and event code will be displayed on the window. Record ID 1 is the latest detected error recorded and record ID 20 is oldest detected error recorded. If there are 20 error on the window and if a new error is detected, then the oldest detected error will be removed from the list and the newly detected error will be added at the top of the list.
Trips
The Trips window provides the list of trip records of the TeSys Tera system.
Up to 20 trip logs with record ID, timestamp, trip cause, value of important settings when the trip occurred, value of measurements recorded when the trip was detected and trip code will be displayed on the window. Record ID 1 is the latest trip recorded and Record ID 20 is oldest trip recorded. If there are 20 trip records on the window and if a new trip is detected, then the oldest trip record will be removed from the list and the new trip record will be added at the top of the list.
Export
The Export function exports the list of records in CSV format.
To export the list of records, select Export, select the destination folder, and select Save.
Refresh
The Refresh function updates the list of records and displays the latest list.
The Data Record node can be updated by selecting Refresh in the connected mode.
Clear Event Logs or Clear Trip Logs
The Clear Event Logs or Clear Trip Logs clears the list of events or trips by selecting Clear Event Logs or Clear Trip Logs in the respective windows.
Device Internal Status
The Device Internal Status window displays the communication and operation status of the different modules of the TeSys Tera system.
Communication Status
The Communication Status window displays the status of the communication parameter of the TeSys Tera system.
When the Ethernet variants of the LTMT main unit is used in the TeSys Tera system, the following subsections are available:
-
Ethernet – Displays the Ethernet Global Statistics, Ethernet Diagnostics Port 1 Statistics, and Ethernet Diagnostics Port 2 Statistics of the LTMT main unit.
-
IP Network Services – Displays the Modbus TCP Port status.
-
Communication Loss Status – Displays the Communication Loss Status of the LTMT main unit.
Trip Counters
The Trip Counters window displays the number of trips per category within the TeSys Tera system.