DOCA0275EN-01

User Map

The User Map variables are designed to optimize the read and write registers.

The following procedure describes how to set user map addresses:

  1. Select User Map in the tree view:

    • Addresses are ranked from 1 to 100.

    • Addresses are divided into four groups.

  2. Enter an address value in the table:

    • The entered address must be in the decimal format and should be from 0 to 9249.

    • Enter the address 0 to remove the address from the user map.

  3. Press ENTER to validate the new address:

    • If the address is accepted, the address is added to the user map.

    • If the address is not accepted, the previous accepted address is kept in the user map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?