DOCA0275EN-01

Deleting or Duplicating Objects

Overview

Sometimes it may be necessary to delete a block or duplicate a block in the workspace.

Deleting Blocks

The following procedures describe how to delete one or more blocks:

  1. Select the block(s) to be deleted.

    Result: The selected blocks are highlighted with an orange outline.

  2. Press the DELETE key or select Device > FB Diagram > FBD Editor > Delete.

    Result: The selected blocks are deleted.

  1. Select the block(s) to be deleted.

    Result: The selected blocks are highlighted with an orange outline.

  2. Right-click on the selected block and select Delete.

    Result: The selected blocks are deleted.

Cut, Copy, or Paste Blocks

The following procedure describes how to cut, copy, or paste one or more blocks :

  1. Select the block(s) to be modified.

    Result: The selected blocks are highlighted with an orange outline.

  2. Select Device > FB diagram > FBD editor and select one of the following commands:

    • Copy

    • Cut

    • Paste

    Result: Cut deletes the selected blocks and stores them in the clipboard. Copy duplicates the selected blocks in the clipboard and Paste duplicates the clipboard contents on the workspace.

    NOTE: The keyboard shortcuts CTRL+C, and CTRL+V can also be used to copy the selected blocks and paste them.

Hide or Show Blocks

The following procedure describes how to hide one or more blocks :

  1. Select the block(s) to be hidden.

    Result: The selected blocks are highlighted with an orange outline.

  2. Right-click on the selected block(s) and select Hide/Show.

    Result: The selected blocks are hidden and as displayed as follows:

  3. The list of hidden block are displayed under Hidden Blocks as shown below:

NOTE: When multiple blocks are selected, all the blocks are grouped in the same block.

The following procedure describes how to show one or more hidden blocks :

  1. Right-click on the hidden block(s) and select Hide/Show.

    Result: The selected blocks are Shown.

  2. Alternatively, right-click on the hidden blocks under Hidden Blocks section and select Hide/Show.

    Result: The selected blocks are shown.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?