DOCA0275EN-01

Starter Types

Overview

The FBD editor allows the use of starter block accessible through the Starter Types bar in the Toolbox:

Block

Description

Direct Online

Reversible Direct Online

Star Delta

Overload

NOTE: Placing cursor over the icon will reveal a tool tip defining the icon. This will help you distinguish which type of block is represented by that icon.
NOTE: Only one type of starter can be used at a time.

Direct Online

Using the block sets the starter type as Direct Online.

FBD Display

Arguments

Description

Digital input signal

  • DI1 (5629.0): Local-START> DI

  • DI2 (5629.1): Local-STOP DI

  • DI3 (5629.3): DI Mode Selection 1

  • DI4 (5629.6): Remote-START> DI

  • DI5 (5629.7): Remote-STOP DI

  • DI6 (5629.9): DI Mode Selection 2

  • DI7 (5629.12): Run DI

HMI signals

  • HMI1 (9875.0): HMI_START

  • HMI2 (9875.12): HMI_STOP

  • HMI3 (9875.2): HMI Mode Selection 1

  • HMI4 (9875.4): HMI Mode Selection 2

Communication signals

  • RI1(704.0): COMM Start

  • RI2 (704.2): Remote Mode Selection 1

  • RI3 (704.4): Remote Mode Selection 2

  • RI4 (704.12): COMM Stop

Output signal

  • OP1 (32.0): CL Run1 Cde information

Overload

Using the block sets the starter type as Overload.

FBD Display

Arguments

Description

OP1

Output signal 1

Reversible Direct Online

Using the block sets the starter type as Reversible Direct Online.

FBD Display

Arguments

Description

Digital input signal

  • DI1 (5629.0): Local-START> DI

  • DI2 (5629.1): Local-STOP DI

  • DI3 (5629.3): DI Mode Selection 1

  • DI4 (5629.4): Local-START< DI

  • DI5 (5629.6): Remote-START> DI

  • DI6 (5629.7): Remote-STOP DI

  • DI7 (5629.9): DI Mode Selection 2

  • DI8 (5629.10): Remote-START< DI

  • DI9 (5629.12): Run DI

HMI signals

  • HMI1 (9875.0): HMI_START >

  • HMI2 (9875.12): HMI_STOP,

  • HMI3 (9875.1): HMI_START <

  • HMI4 (9875.2): HMI Mode Selection 1

  • HMI5 (9875.4): HMI Mode Selection 2

Communication signals

  • RI1(704.0): COMM Start >

  • RI2 (704.1): COMM Start <

  • RI3 (704.2): Remote Mode Selection 1

  • RI4 (704.4): Remote Mode Selection 2

  • RI5 (704.12): COMM Stop

Output signal

  • OP1 (32.0): CL Run1 Cde information

  • OP2 (32.1): CL Run2 Cde information

Star Delta

Using the block sets the starter type as Star Delta.

FBD Display

Arguments

Description

Digital input signal

  • DI1 (5629.0): Local-START> DI

  • DI2 (5629.1): Local-STOP DI

  • DI3 (5629.3): DI Mode Selection 1

  • DI4 (5629.6): Remote-START> DI

  • DI5 (5629.7): Remote-STOP DI

  • DI6 (5629.9): DI Mode Selection 2

  • DI7 (5629.12): Run DI

HMI signals

  • HMI1 (9875.0): HMI_START >

  • HMI2 (9875.12): HMI_STOP,

  • HMI3 (9875.2): HMI Mode Selection 1

  • HMI4 (9875.4): HMI Mode Selection 2

Communication signals

  • RI1(704.0): COMM Start >

  • RI2 (704.2): Remote Mode Selection 1

  • RI3 (704.4): Remote Mode Selection 2

  • RI4 (704.12): COMM Stop

Output signal

  • OP1 (32.0): CL Run1 Cde information

  • OP2 (32.1): CL Run2 Cde information

  • OP3 (32.2): CL Run3 Cde information

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?