DOCA0275EN-01

Factory Reset

Overview

The Factory Reset function allows you to reset the TeSys Tera system parameters to its default values.

@Updated Draft 5

NOTE: Factory Reset functionality through TeSys Tera DTM is supported for the Ethernet variants if the LTMT main unit is connect through serial interface (HMI Port).

Performing Factory Reset Command

To performing factory reset command, follow the below steps:

NOTE: Factory reset function works only in connected mode.
  1. Select Device > Factory Reset > Factory Rest Command as shown in the image below.

  2. A confirmation pop-up message will appear after selecting the command.

NOTE: The TeSys Tera DTM Library will be disconnected from the TeSys Tera system after execution of this command.

When the Factory Reset command is executed, the function restores the configuration of the TeSys Tera system to the factory settings and restarts the TeSys Tera system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?