DOCA0275EN-01

Logic Simulator

Overview

The Logic Simulator tab is used to display the LTMT main unit Logic Simulator which enables you to test the functioning of a custom logic program.

For more information about the Logic Simulator, refer to LTMT Main Unit Logic Simulator.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?