Add Element

This tool allows you to add new commands, dockable windows, extensions, etc. Click Add to launch the wizard.

  1. Click Add.
  2. Browse to and select a type library that contains the element(s) you want to add. The following file types are accepted: *.olb, *.tlb, *.exe, and *.dll. Click Open.
  3. Once you have selected a type library, you may view its contents and select those to be added. The figure below shows the Select Components list. Select checkboxes to add components. Click Add.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.