Begin Construction

Executes the Construct Work Request task on the design’s parent work request if it is necessary.

Enabled

  • MMWorkflowManager must be the current extension.

  • The node passed to this subtask is a design node.

Execute

  • If the ConstructOnApprove configuration value is false, the subtask gets the design’s parent and checks to see if it is a work request. If the parent node is a work request, the Construct Work Request task is executed on the parent node to set its state to In Construction.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?