Upgrade to 10.1.1 and Later

With release 10.1.1, changes were made to support Mobile functionality. The following upgrade is necessary only if you wish to implement Mobile.

These instructions are intended for GIS administrators who currently are in production with Workflow Manager and who want to upgrade to the most recent release of the ArcFM Solution. This document does not apply if you are not currently using Workflow Manager and will be implementing it with the most recent version of the ArcFM Solution (i.e., you are new to ArcFM and are starting with the most recent release). If this is the case, refer to Set Up Workflow Manager.

If you are upgrading your Process Framework, you might also need to use the Process Framework Administration Upgrade Tool.

Mobile

If you want to implement Mobile, you need to execute Create Table Indices after tables have been added to the database.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.