Incremental Copy Design

Copies a design but NOT its compatible units.

Enabled

  • The node passed to this subtask is a design node.

  • The design has been opened in ArcMap and saved (creating an associated version).

  • The WMSUseWRVersions value in the MM_PX_CONFIG table is set to 0. If this value is set to 1 the subtasks is disabled.

Execute

  1. Creates a new work request.

  2. Copies the design node to the new WR. Any CUs associated with the design are NOT copied.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?