Local Implementation with IIS7

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Follow the steps in this section if your web service does not require access to the network and you're using version 7 of IIS Manager.

Replication Web requires ASP.NET and all supporting components, including .NET Extensibility, ASP.NET, ISAPI Extensions, and ISAPI Filters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.