Upgrade Session Manager

These instructions are intended for GIS administrators who currently are in production with Session Manager and who want to upgrade to the most recent release of the ArcFM Solution. This document does not apply if you are not currently using Session Manager and will be implementing it with the most recent version of the ArcFM Solution (i.e., you are new to ArcFM and are starting with the most recent release). If you are installing Session Manager for the first time, refer to Set Up Session Manager.

If you are upgrading your Process Framework, you might also need to use the Process Framework Administration Tool.

When upgrading from an older release, you must perform all upgrades between your old version and the release you're installing. For example, if you are upgrading from 8.3 to 8.3.2, you must perform the upgrades for 8.3.1 and 8.3.2.

  • No additional upgrade required for 10.6.1

  • No additional upgrade required for 10.2.1d + SP3

  • No additional upgrade required for 10.2.1c + SP3

  • No additional upgrade required for 10.2.1b + SP1

  • No additional upgrade required for 10.2.1a + SP1

  • No additional upgrade required for 10.2.1

  • No additional upgrade required for 10.2

  • Upgrade to 10.1.1

  • No additional upgrade required for 10.1

  • No additional upgrade required for 10.0.3 SP1

  • No additional upgrade required for 10.0.3

  • No additional upgrade required for 10.0.2

  • No additional upgrade required for 10.0.1 SP1

  • No additional upgrade required for 10.0.1

  • No additional upgrade required for 9.3.1  SP1

  • No additional upgrade required for 9.3.1

  • Upgrade to 9.3 Rev2

  • No additional upgrade required for 9.3 SP1

  • No additional upgrade required for 9.3

  • No additional upgrade required for 9.2.1

  • Upgrade to 9.2

  • No additional upgrade required for 9.1.2 SP1

  • Upgrade to 9.1.2

  • No additional upgrade required for 9.1 SP1

  • Upgrade to 9.1

  • No additional upgrade required for 9.0.1 SP1

  • Upgrade to 9.0.1

  • No additional upgrade required for 8.3.2

  • Upgrade to 8.3.1

    IMPORTANT: If your workflow is the same as the one provided with the Minerville sample data, you can use the Process Framework Administration Tool Import/Export tab to export the sample workflow and import it into your database instead of performing the upgrades described in this section. This replicates the sample workflow. Any customizations are lost. The Process Framework Administration tool is not installed with ArcFM Engine products. If your upgrade requires the use of this tool, it must be done using a machine on which ArcFM Desktop has been installed in order to access this tool.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.