Feature-Linked Annotation Layers

If you have feature-linked annotation layers, remove the Auto-Create ESRI property on your backdrop geodatabase. Otherwise, you will end up with duplicates when doing mobile transport.

  1. In ArcCatalog, right-click the feature and select Properties.
  2. Select the Annotation tab.
  3. Ensure that Create annotation when new features are added and Update annotation when feature's shape is modified are unchecked.
  4. Click OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.