Add MIME Type to IIS Using IIS7

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

This step ensures that the IIS recognizes the .delta and .xip files transmitted by the Web Service to the client.

  1. Open the Internet Information Services (IIS) Manager and select your machine name.
  2. In the middle pane double click MIME Types.

  3. This displays a list of MIME Types in IIS7. Look for the following types in the list. If they don't exist, click Add in the Actions column to add them.

    .delta

    application/octet-stream

    .xip

    application/octet-stream

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.