Engine Mobile Designer

Engine Mobile Designer provides the mobile user with Designer functionality while in the field. The user can receive, create and edit designs, then send them to the enterprise.

Required Licenses in the Field: Designer

Field Databases: Backdrop, Workflow Manager

Perform the following steps to configure Designer in the field.

Step 1: Set Up Directory Structure

Step 2: Configure Graphic Annotation

Optional. Perform this configuration if you wish to store graphics in an annotation layer.

Step 3: Create Backdrop Database

Step 4: Create Workflow Manager Databases

Step 5:  Create Replicas 

Step 6: Set Up Mobile Synchronizer

Step 7: Deploy to Multiple Client Machines

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.