Archive Packets

Compresses the mobile packet using the selected encoder. If Archive fails on any nodes in the list, the subtask will continue with subsequent nodes. Other subtasks within the task will continue to fire as normal.

Enabled

  • The node passed to this subtask must not be locked.

Execute

  1. Compresses the packets associated with the current node and its children using the transporter's "encoder." If a node is locked, it will not be archived. A message will be sent to the event log and the subtask will continue to the next node.

  2. A message indicates to the user any locked nodes that weren't archived.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?