Configure Replication Server

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

The replication server runs a service that periodically receives updates from the SDE geodatabase. Perform the steps in this section to configure the replication server. The first two steps, Create Base Path and Update Replication Server Service Login involve the domain user created in the Before You Begin section. Before starting configuration, ensure this domain user has been created. Refer to the Geodatabase Replication Read Me for hardware and software requirements.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.