Change Owner All Session
Changes the owner of a session to any valid user.
Enabled
-
MMSessionManager must be the current extension.
-
The node passed to this subtask must be a session.
-
Determines if there are any other users that have a role that can access the node in its current state.
Execute
-
Identifies the users with the appropriate roles assigned to own the selected node.
-
Gets the value of the DefaultUser parameter.
-
If the AutoChangeOwner value is set to 1 (True), selects the DefaultUser and assigns the node. If no DefaultUser value is set, allows the user to select from a list of valid users.
-
If the AutoChangeOwner value is set to 0 (False), selects the DefaultUser and allows the user to change the selection from a list of valid users. If no DefaultUser value is set, allows the user to select from a list of valid users.
-
Assigns the node to the chosen user.
Parameters
-
DefaultUser: takes a user name as a value. The default value is null.
- AutoChangeOwner: takes a value of 0 or 1. 0=False, prompt the user to select owner; 1=True, select default owner without prompt. The default value is 0 (False).