Set Active Graphics Layer

Sets the Active Annotation Target according to the user-defined parameter.

Enabled

  • Enabled if Process Framework is running through ArcMap or ArcFM Viewer for ArcGIS Engine.

Execute

  • Sets the Active Annotation Target using the Graphics Layer Name entered as the subtasks parameter.

Parameters

  • TargetGraphicsLayerName: takes a string value Active Annotation Target. If this parameter is not set, it will default to the first annotation layer in the pull-down list.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?