ArcFM Viewer for ArcGIS Engine

Engine Mobile provides all the functionality of the enterprise while in the field. The mobile user has full editing capabilities, and can create or delete features while in the field.

Required Licenses in the Field: ArcFM

Field Databases: Backdrop, Login (optional), Session Manager

Perform the following steps to configure Engine Mobile in the field.

Step 1: Set Up Directory Structure

Step 2: Configure Graphic Annotation

Optional. Perform this configuration if you wish to store graphics in an annotation layer. 

Step 3: Create Backdrop Geodatabase

Optional: Create Login Database

The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.

Step 4: Create Session Manager Database

Step 5: Create Replicas

Step 6: Set Up Mobile Synchronizer

Step 7: Deploy to Multiple Client Machines

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.