Re-send Design to Field

Executes the Send to Field task if the node’s current owner has the Mobile role assigned.

Enabled

  • MMWorkflowManager must be the current extension.

  • The selected node must be a design.

Execute

  1. Gets the node's owner.

  2. Executes the Send Design to Current Field Owner task if the node's owner has the Always Mobile role assigned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?