Geodatabase Replication - Before You Begin

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Before configuring Geodatabase Replication, there are several things to consider. Be sure to review the appropriate Geodatabase Replication ReadMe file for complete system requirements.

  1. Identify the servers on which the GDB Replication Server and Web Service Geodatabase Replication components are to be installed. Those two components can be installed on the same server or on separate servers. 
  2. Determine the Base Path on the server and create a directory (ServerBase, in the example). The Base Path is where the geodatabases retrieved from the SDE sync version are stored. The Web Service uses these geodatabases to create a delta file (see Overview). The Base Path and Geodatabase Replication Server may reside on the same or different servers.
  3. Determine the Client Base Path. All client machines will have a Client Base Path. This directory is discussed in the Configure Client topic.
  4. Ask your Windows Domain Administrator to create a domain user, which is ONLY necessary if your web service resides on a machine other than the replication server. This domain user executes the Geodatabase Replication Server service. This user must have GDBR directory permissions on the server base path to delete files created by the user who previously ran replication. This user must also have ArcFMGDBReplicationService directory permissions assigned on the web service. You can name this domain user according to your standard naming convention.
    TIP: Occasionally this help file may refer to the term "Bootstrap." Bootstrap is a specific situation in which you get a full download. A bootstrap differs slightly depending on whether you're updating the client or the server.
    • Client: A bootstrap may be necessary when no replica version exists on the client. Geodatabase Replication gets a full download (aka bootstrap) using the latest version available on the Server for the selected replica.
    • Server: When bootstrapping on the Server, Geodatabase Replication uses the Initial Extract version to get all changes made to the geodatabase since the Initial Extract version was created.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.