Assign ArcFMGDBReplicationService Directory Permissions

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

This step must be performed if you're doing a distributed implementation. The domain user’s group must have permissions to the ArcFMGDBReplicationBase directory and to C:\Windows\Temp. The ArcFMGDBReplicationService directory is created when ArcFM Geodatabase Replication Web is installed.

  1. In Windows Explorer, browse to the ArcFMGDBReplicationService directory (C:\Inetpub\wwwroot\ArcFMGDBReplicationService by default).
  2. Right-click ArcFMGDBReplicationService and select Properties.
  3. On the Security tab click Edit.
  4. This displays the Permissions window. Click Add.
  5. Add the IIS_WPG or IIS_IUSRS user group (e.g., domain\IIS_WPG or domain\IIS_IUSRS).
  6. Assign the user or group the following permissions: Read & Execute, List Folder Contents, Read. Optionally: Write, Modify.
  7. Click OK.
  8. Perform these steps again to assign the same permissions for the same user/group to the C:\Windows\Temp directory.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.