Create Replicas

This step is necessary only if you're using Geodatabase Replication.

In this step, you'll set up the Geodatabase Replication replicas necessary to maintain the backdrop database as well as move sessions or designs between the field and Enterprise.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?