Create Work Request

Adds a new work request node.

Enabled

  • MMWorkflowManager must be the current extension.

  • Workflow Manager must be open and visible.

  • The selected node is a TopLevel node.

Execute

  1. Creates a new work request.

  2. Sets these properties on the work request: default work request name and description, and current owner.

  3. Adds the node to the Tree.

  4. Sets the node’s build object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?