Advanced Redliner

This implementation expands upon the Basic Redliner functionality. It offers the option of placing redline graphics as annotation. Graphics placed as annotation can be sent to the enterprise and posted to the geodatabase.

Required Licenses in the Field: Redliner Extension and ArcFM Viewer for ArcGIS Engine or ArcFM Viewer

Field Databases: Backdrop, Login (optional), Process Framework (e.g., Session Manager or Workflow Manager)

Perform the following steps to configure Advanced Redliner.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.