Mobile Submit Session

Changes the mobile session’s status to Pending Approval and allows the mobile user to assign it to an approval officer.

Enabled

  • MMSessionManager must be the current extension.

  • The node passed to this subtask must be a session.

  • The Submit Session task must be enabled.

Execute

  • Executes the Submit Session task.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?