Upgrade Session Manager/Workflow Manager

If you are upgrading from a previous version of Process Framework, you may need to utilize the Process Framework Database Upgrade tool (PxDatabaseUpdater.exe). You may also need to add tasks, roles, etc., using the Process Framework Administration Tool. To do this, follow the upgrade Session Manager or upgrade Workflow Manager procedures to upgrade to the appropriate version.

This section also contains descriptions of the subtasks utilized by Process Framework and its extensions.

Process Framework Subtasks

Session Manager Subtasks

Workflow Manager Subtasks

Password Protection: ArcFM supports user-level security on Access databases. When connecting to a secure Access database, just enter the proper user name and password on the Process Framework login screen. If there is no user level security on the Access database, only a user name is required. Secure Access databases are supported when they contain only Process Framework information. Note that password-protected Access databases are NOT supported by Esri. Access geodatabases cannot be password-protected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.