Enable Directory Browsing Using IIS7

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Both local and distributed implementations with IIS7 require that you enable Directory Browsing. Follow the steps below. 

  1. Open Computer Management.
  2. Expand Services and Applications and select Internet Information Services (IIS) Manager.
  3. In the Connections column, expand the local machine name > Sites >Default Web Site and select ArcFMGDBReplicationService.
  4. In the next column, double click Directory Browsing in the IIS category. Alternately, you can select Directory Browsing and click Open Feature at the top of the far right column.

  5. Click the Enable link in the far right column to enable Directory Browsing.

  6. If you're using BITS, perform the above steps for ArcFMGDBReplicationBase as well. This is the virtual directory created in the Create Virtual Directory step.
  7. Close Computer Management.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.