Is Session in a Non-Mobile State?

Determines if the session is open.

Enabled

  • If the state is 8 (Mobile), returns false.

Execute

  • Always returns true.

Parameters

  • OverrideDefaultMobileStateNumber: takes a long integer for the number that corresponds with the session's current state. The default is 8 (Mobile).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?