ArcFM Engine Administrator

This stand-alone application allows a system administrator to configure various aspects of ArcFM Viewer for ArcGIS Engine. The ArcFM Engine Administrator provides login information for ArcFM Viewer for ArcGIS Engine. It also provides an administrator with the ability to determine which layout elements are available to users (e.g., commands, dockable windows and extensions). The Layout tab also allows you to determine application license selection.

Access the ArcFM Engine Administrator in the Start menu > ArcFM Solution > Admin > ArcFM Engine Administrator, or in the ArcFM Solution\Bin directory (ArcFMEngineAdminTool.exe). This tool is installed with ArcFM Viewer for ArcGIS Engine.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.