Backdrop Database

Use a geodatabase replica to keep the backdrop database in the field synchronized with the Enterprise database.

The backdrop database (e.g., Backdrop.mdb) should reside on the server machine in the initial extract directory. Geodatabase Replication may use this copy to do a bootstrap update if necessary.

A copy of this database should also reside on the administrator machine. Open the database in ArcMap on this machine and ensure the stored display layers are connected. Once the stored display is properly displayed, save it and copy the database to the same directory on the client machines (e.g., C:\ReplicationField\Backdrop).

To configure a geodatabase replica to maintain the backdrop database, follow the steps outlined on the following pages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.