Send to Field

Takes a design from the enterprise server and puts it in the mobile environment.

Enabled

  • The Database ID field must have a value. This field is located in the Process Framework Administration Tool on the Extensions tab.

  • MMWorkflowManager must be the current extension.

  • The selected node must be a design.

  • The MM_Mobile_State table must exist in the current Process Framework database.

  • The current design must have not already been imported.

  • Another design cannot be approved for this design's work request.

Execute

  1. Creates a mobile packet if one does not already exist.

  2. Closes the design if it is open in ArcMap.

  3. Saves the mobile packet.

  4. Adds the mobile packet to the transporter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?