Update Replication Service Login

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

This step is necessary only if you are using Geodatabase Replication

The domain user created when following the steps in the Before You Begin topic is used to run the Geodatabase Replication Server Service. This step gives the domain user access to log in to the service.

  1. On the replication server, open Computer Management.
  2. Expand Services and Applications.
  3. Select Services.
  4. In the right-side pane, right-click ArcFM Geodatabase Replication Service and select Properties.
  5. Select the Log On tab.

  6. In the This Account fields, type the domain user and password.
  7. Click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.