Is Mobile Solution Enabled?

Determines if Mobile is enabled.

Enabled

  • Mobile is enabled for process framework only if the process framework enterprise value is set on both the field and enterprise.

  • On a field machine, a Field Working Directory must exist. On the enterprise, an Enterprise Working Directory must exist.
  • The subtask looks for the ProcessFrameworkEnterprise configuration value in the Process Framework Administration tool.
  • On a field machine, it looks for the ProcessFrameworkField configuration value or a ProcessFrameworkField directory at the default location.

Execute

  • Always returns True.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?