Create Session Manager Databases

Configure Enterprise Process Framework Database

Configure Field Process Framework Database

IMPORTANT: Step 5 includes how to create a Process Framework replica that sends/receives sessions and designs. Step 6 discusses how to set up the Mobile Synchronizer. You need only one of these methods. If you elect to use the Mobile Synchronizer for sending/receiving, then you may still want to review the Create Replicas step in case you wish to use Geodatabase Replication to maintain your backdrop database in the field.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.