Server (Enterprise) with Geodatabase Replication

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Create the following directories on the server or Enterprise machine. These directories do not have to be named exactly as shown. 

  • ReplicationServer: This is the Server Base Directory used by Geodatabase Replication to send/receive sessions and designs. It also uses this directory to maintain the backdrop database and the login database.

  • InitialExtract: This directory contains all initial extract databases for all replicas. For Engine Mobile, this will be one or more backdrop replicas. You can break the backdrop into regions (e.g., Northwest, Southeast). This results in multiple backdrop databases (one for each region) and multiple backdrop replicas (one for each database).

  • ProcessFramework: This directory must be created by an administrator on the Enterprise machine and be available for all client machines to access. It provides the necessary directory structure to transport Engine Mobile sessions and designs between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkEnterprise value) in the Process Framework database that points to this directory. All other folders shown in this directory are created automatically during the initial send/receive. No files in the ProcessFrameworkServer directory should ever be edited manually.

  • Login: This directory stores the optional login database. Use a directory replica to distribute this database to field machines and update it in the field, should the Enterprise version change. If you choose not to use a login database (recommended), then you don’t need this directory.

    TIP: The login database is optional. Schneider Electric recommends adding the necessary stored display and graphic favorites to the Backdrop database to eliminate the need for a Login database.

Once you have the directory structure set up on the server (Enterprise) machine, you need to assign permissions to the ReplicationServer and ProcessFramework directories.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.