Submit Design

Changes the design’s status to Pending Approval and allows the user to assign it to an approval officer.

Enabled

  • MMWorkflowManager must be the current extension.

  • The selected node is a design node.

  • There may not be another approved design in the same work request. If there is another approved design, the subtask is disabled.

Execute

  1. Prompts the user to select an approval officer.

  2. Attempts to transfer ownership.

  3. Tells the builder that the user has changed so it can update the tree if necessary.

  4. If ownership is changed, the design is closed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?