Inspector

The Inspector extension is available only in ArcFM Viewer for ArcGIS Engine. It allows the user to edit non-spatial attributes, and create, update, and delete related objects in the field. This implementation also includes the ability to place redline graphics (either as simple graphics or as annotation). The Inspector tool makes it easy for mobile users to perform inspections (e.g., pole inspections) and manage related objects.

Required Licenses in the Field: Inspector Extension and ArcFM Viewer for ArcGIS Engine

Field Databases: Backdrop, Login (optional), Session Manager

Perform the following steps to configure Inspector.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.