Engine Mobile Directory Structure - No Geodatabase Replication

This directory structure is necessary if you're planning to use Mobile Synchronizer to send/receive sessions and designs and do not plan to use Geodatabase Replication to maintain the backdrop database in the field.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?