Verify Design

Posts the design and changes the work request’s state to Complete before removing it from the Tree. Completed work requests may be viewed using the Completed Work filter.

Enabled

  • MMWorkflowManager must be the current extension.

  • The selected node is a design node.

  • The user must have an editing session started in ArcMap and have a design open.

  • The user must be able to post if using a versioned database.

Execute

  1. Post the design.

  2. Transitions the design’s parent work request to Complete by executing the Complete Work Request task.

  3. Sets the work request node to hidden.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?