Create Login Database 

The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.