System Requirements

In order to access the Process Framework on an enterprise database system (non-MS Access database), the appropriate database client must be installed on the user’s machine. Refer to the appropriate ArcFM Desktop ReadMe version file for your current release for system requirement information.

Process Framework supports both Oracle and Microsoft SQL Server databases. Scripts are provided with the install of ArcFM and Designer that creates the system tables required by the Process Framework. SQL scripts are located in the Documentation/Process Framework Enterprise/MS-SQL directory of the ArcFM Solution installation folder. Oracle scripts are located in the Documentation/Process Framework Enterprise/Oracle directory of the ArcFM Solution installation folder.

Sample Data: A sample Access database for Session Manager is provided with ArcFM (SessionManager.mdb). The Designer installation includes a sample Access database for Workflow Manager (WorkflowManager.mdb). Both sample databases are located in Sample Data/Databases of the ArcFM Solution installation folder. You can use the Process Framework Administration Tool to export an XML file from either of these sample databases, and import into your own Process Framework database.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.