Reconcile Session

Reconciles the session’s version with the geodatabase.

Enabled

  • Session Manager must be opened through ArcMap.

  • A session node must be open in ArcMap.

  • The session must be editable.

  • The workspace must be versioned.

Execute

  1. Determines whether the DefineConflictsByColumn configuration value is set in the Process Framework Admin Tool (Configuration tab). If this value is set to 1, conflicts are defined by column. If this value is set to 0 or not set at all, conflicts are defined by row.

  2. Reconciles the session node. If reconcile fails or is cancelled, Execute returns false and the subtask is rolled back along with any subtasks executed prior to it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?